EIO0000005638.01

End of Life (WEEE)

The product contains electronic boards. It must be disposed of in specific treatment channels. The product contains cells and/or storage batteries which must be collected and processed separately when they have run out and at the end of product life (Directive 2012/19/EU).

The cells or batteries installed in the product do not contain a weight percentage of heavy metals over the threshold notified by European Battery Regulation 2023/1542.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?