EIO0000005638.01

Precautions for Building into an End-use Product

This product is designed for use on flat surfaces of enclosures. The front surface is rated for IP65 enclosure.

Be aware of the following when building this product into an end-use product:

  • The rear face of this product is not approved as an enclosure. When building this product into an end-use product, be sure to use an enclosure that satisfies standards as the end-use product's overall enclosure.

  • Install this product in an enclosure with mechanical rigidity.

  • This product is not designed for outdoor use.

  • Install and operate this product with its front panel facing outward.

NOTE: The necessary torque is 0.5 N•m (4.4 lb-in).
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?