Installation Procedure
This section describes how to install this product to the panel.
DANGER |
|---|
|
HAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASH
Failure to follow these instructions will result in death or serious injury.
|
| NOTICE |
|---|
|
EQUIPMENT DAMAGE
Failure to follow these instructions can result in equipment damage.
|
| NOTICE |
|---|
|
BROKEN
ENCLOSURE
Do not exert more torque than the amount specified.
Failure to follow these instructions can result in equipment damage.
|
- Check that this product's gasket is seated securely into
the bezel's groove, which runs around the perimeter of the display
panel frame.NOTE: Always use the installation gasket, since it absorbs vibration in addition to repelling water.
- Based on this product's Panel Cut Dimensions, open a mount-hole on the panel and attach this product to the panel from the front side.
- Insert the installation fastener into the insertion slots of this product.
- In a clockwise direction, tighten the installation fastener's screws with a screwdriver. The necessary torque is 0.5 N•m (4.4 lb-in).
DANGER