990-5997E-001

Installation Procedure

NOTE: The illustrations in this manuals shows the installation in a 700 mm empty battery cabinet. The battery breaker kit can also be installed in a 1100 mm empty battery cabinet or in a grounded metal box.
  1. Mount the battery breaker kit. Follow one of the procedures:
  2. Connect the Signal Cables.
  3. Connect the Power Cables.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.