990-5992G-001

Clearance

NOTE: Clearance dimensions are published for airflow and service access only. Consult with the local safety codes and standards for additional requirements in your local area.

Option A

NOTE: If the UPS is installed without side access, the length of the cables connected to the UPS must allow for rolling out the UPS.

Option B

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.