990-5992G-001

Recommended Bolts and Cable Lugs

Cable size (mm²) Bolt size Cable lug type
16 M8 KST TLK16-8
25 M8 KST TLK25-8
35 M8 KST TLK35-8
50 M8 KST TLK50-8
70 M8 KST TL70-8
NOTE: If the recommended lug type is not available, use a local M8 lug type as a substitute.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.