990-5992G-001

Communication Interfaces

Rear View of the UPS

  1. RS485

  2. USB

  3. Dry contacts

  4. CAN_R: CAN termination resistor

  5. Parallel ports

  6. Load bus synchronization port

  7. EPO

  8. Cold start button (optional)

  9. Network management card (NMC)

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.