990-5992G-001

Receiving

External Inspection

When the shipment arrives, inspect the shipping material for any signs of damage or mishandling. Do not attempt to install the system if a damage is apparent. If any damage is noted, contact Schneider Electric and file a damage claim with the shipping agency within 24 hours.

Compare the components of the shipment with the bill of lading. Report any missing items to the carrier and to Schneider Electric immediately.

Verify that labelled units match the order confirmation.

Remove the UPS from the Pallet

  1. Move the UPS to the final installation area using a forklift.
  2. Remove the shipping materials and the ramp from the UPS.
  3. Loosen the bolts and remove the shipping brackets. Save the bolts for the ramp and dispose of the shipping brackets.
  4. Place the ramp on the pallet and fasten with the bolts from the shipping bracket.
  5. Roll the UPS down from the pallet.
  6. Move the UPS to its final location and use a wrench to lower the levelling feet. Ensure that the cabinet is level.
  7. Lock the wheels.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.