990-5995E-001

Replace the Air Filter

  1. Open the front door of the UPS.
  2. Loosen the screws and remove the metal brackets.
  3. Replace the dust filter.
  4. Reinstall the metal brackets and fasten with the screws.
  5. Close the front door.
  6. Reset the air filter counter in the display.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?