990-5995E-001

Location of Breakers and Switches

60-100 kVA 400 V/50 kVA 208 V UPS for External Batteries

 

120-160 kVA 400 V/60–80 kVA 208 V UPS for External Batteries

200 kVA 400 V/100 kVA 208 V UPS for External Batteries

Front View of the 60 kVA 400 V UPS for Internal Batteries

Front View of the 80 kVA 400 V UPS for Internal Batteries

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.