990-5995E-001

Configure the UPS Settings

NOTICE
risk of equipment damage
Only trained personnel following the required training must make modifications to the UPS system parameters.
Failure to follow these instructions can result in equipment damage.
  1. From the home screen of the display select Settings > Advanced settings > System settings.
  2. Set the System mode. Choose between:
    • Choose ECO mode to use static bypass mode as the preferred operation mode.
    • Choose Single mode for a single UPS.
  3. Tap Save settings.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.