990-5995E-001

Transfer a Single UPS from Static Bypass Mode to Normal Mode

NOTE: The UPS will normally transfer automatically from static bypass to normal mode. This procedure can be used to manually transfer to normally mode if the bypass frequency or voltage is above the specified limits.
  1. From the home screen of the display select Control > Inverter ON.

    The LEDs on the user interface show as follows:

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.