990-5995E-001

Configure the Battery Settings

  1. From the home screen of the display select Settings > Advanced settings > Battery settings and configure the following settings.
    1. Number of battery strings: Set the number of battery strings in the battery solution.
    2. Battery blocks per string: Set the number of battery blocks in one battery string.
    3. Battery block capacity (Ah): Set the rated capacity of the battery block.
    4. Periodic boost charge (M): Set the interval in months for changing from float charge to boost charge.
  2. Tap arrow down and complete the following settings:
    1. Maximum charge current: Choose a value between 0.05 and 0.15 C.
    2. Float voltage (V): Choose a value between 2.20 and 2.29
    3. Boost voltage (V): Set the upper limit for the boost charge voltage of a battery cell. Choose a value between 2.30 and 2.40.
    4. Boost charge duration (minutes): Set the duration of the boost charge. Choose a value between 0 and 999 minutes.
  3. Tap arrow down and complete the following setting:
    1. Float temp. compensation: Choose a value between 0.000 and 0.007 V/°C per cell.
  4. Tap Save settings.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.