990-5995E-001

Status LEDs

LED State Description
ALARM Steady red Critical alarm
Flashing red Warning alarm
Off No alarm condition
BYPASS Steady yellow The load is supplied by the bypass source
Flashing yellow There is an alarm condition on the bypass source
Off The load is not supplied by the bypass source
BATTERY Steady yellow The load is supplied by the battery source
Flashing yellow The battery source is unavailable
Off The load is not supplied by the battery source
INVERTER Steady green Inverter on
Off Inverter off
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.