990-5995E-001

Status LEDs on the Communication Interface

Front View of the 60-80 kVA 400 V UPS for Internal Batteries

Rear View of 60-100 kVA 400 V/50 kVA 208 V UPS for External Batteries

Front View of 120-160 kVA 400 V/60-80 kVA 208 V UPS for External Batteries

Front View of 200 kVA 400 V/100 kVA 208 V UPS for External Batteries

LED State Description
A. Abnormal Steady red Critical alarm present
Off No critical alarm present
B. Alarm Steady yellow Warning alarm present
Off No warning alarm present
C. Normal Steady green Normal condition
Flashing green Self-testing in progress/UPS is parallel master
Off UPS is off
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.