990-5995E-001

Configure Life Cycle Monitoring

  1. From the home screen of the display select Service > LCM settings.
  2. Set the time in months between air filter checks. The system will generate a Check air filter message when it is time to check the air filters.
  3. Tap Save settings.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.