990-5995E-001

LBS Mode (Optional)

NOTE: LBS mode requires connection of optional synchronization cables. Refer to the installation manual for more information.

When LBS mode is enabled, the output of two independent UPS systems (single or parallel) will be synchronized. Synchronization of the output is not supported when both UPS systems are in static bypass mode or maintenance bypass mode.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.