ESXFEUG003EN-01

Duplicating and Updating a Tariff

Copying and Pasting a Tariff

Follow these steps to copy and paste an existing tariff:

  1. On EcoStruxure Facility Expert, select Settings > Utility and Tariff Settings > Utilities and Tariffs.

  2. Select a tariff to copy and click the copy icon.

    Result: The Copy Tariff window opens.

  3. In the Copy Tariff window:

    • Enter a name for the new tariff.

    • Select a utility to which the tariff applies.

  4. Click OK.

    Result: The new tariff is added to the Utilities and Tariffs view.

Updating Prices

Follow these steps to change a tariff price:

  1. On EcoStruxure Facility Expert, select Settings > Utility and Tariff Settings.

  2. Select a tariff to update, and then in Tariff Price click + to create a new valid date.

  3. Update the rates.

  4. Click Save.

    NOTE: To view rates for a previous period, select the period in the Valid from drop-down list.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.