Architecture with PrismaSeT Active Wireless Panel Server
The following topic presents a typical PrismaSeT Active architecture with Wireless Panel Server using LoRa communication.
The Wireless Panel Server is a gateway embedded in the roof of PrismaSeT P Active or PrismaSeT G Active switchboards, enabling wireless connectivity to Schneider Electric cloud.
The Wireless Panel Server offers the following advantages and services:
-
Switchboard voltage loss monitoring
-
Fire prevention in electrical distribution switchboards
-
Power availability alarming
-
Energy consumption management
The Wireless Panel Server provides monitoring of the switchboard via EcoStruxure Facility Expert software.
The Wireless Panel Server provides the following features:
-
Voltage presence indicator, locally with the Wireless Panel Server LEDs.
- Voltage loss detected in the switchboard:
-
Locally with the Wireless Panel Server LEDs.
-
Remotely by notifications on mobile devices (smartphone or tablet).
-
-
LoRa communication enables voltage loss monitoring through long range communication.
- IEEE 802.15.4 wireless communication enables communication with
wireless devices installed in the switchboard:
-
HeatTag sensors
-
PowerTag Energy sensors
-
Wireless indication auxiliaries for ComPacT NSX and ComPacT NSXm (available beginning 2022)
-
Acti9 Active (available end 2022)
-
-
Remote communication with a smartphone or tablet through Bluetooth® wireless technology.
-
Remote alerts with actionable details through EcoStruxure Facility Expert App - Operations subscription.
-
Continuous monitoring and trends through EcoStruxure Facility Expert App - Energy subscription.
-
Firmware update.
For more information about LoRaWAN protocol, refer to DOCA0203EN PrismaSeT Active - Installation and Maintenance Guide.
The following illustration shows a possible architecture of the Wireless Panel Server.
-
EcoStruxure Power Commission App for wireless devices configuration
-
EcoStruxure Facility Expert cloud-based software for asset and energy management:
-
Voltage loss notification
-
Sensors' alert system through App and webpages (with EcoStruxure Facility Expert - Operations subscription)
-
Energy management through webpages (with EcoStruxure Facility Expert - Energy subscription)
-
Maximum Performance
Supported Wireless Devices
The following table presents the IEEE 802.15.4 wireless devices installed in a PrismaSeT switchboard and able to communicate with the embedded Wireless Panel Server.
More Information
For more information about Wireless Panel Server, visit the product range webpage and refer to the following documents:
Title of documentation | Reference number |
---|---|
PrismaSeT Wireless Panel Server (SMT10015 / SMT10016 / SMT10019) - Instruction Sheet | NNZ50846 |
PrismaSeT Active - Installation and Maintenance Guide | DOCA0203EN |
EcoStruxure™ Power - Commissioning Guide for Digital Solutions based on PrismaSeT Active | ESXP1G005EN |
EcoStruxure Facility Expert Starter Guide for Operations | ESXUG001EN |
How Can I Reduce Vulnerability to Cyber Attacks? | Cybersecurity System Technical Note |