ESXFEUG003EN-01

Performance and Limitation

Com'X Limitation

Characteristics Values

Maximum number of meters

64

Maximum number of variables

200

Features limitation

Monitoring only, no control if using Com'X, PrismaSeT Active or PowerTag Link C as a gateway to cloud.

EcoStruxure Facility Expert Limitation

Characteristics Values

Maximum number of Com'X per site

5

Maximum number of main switchboards per site

5

Recommendations on Dashboard and Energy Widgets

Characteristics Values

Active energy per meter visualization

  • Widget diagram: up to 8 meters

  • Full screen diagram: up to 20 meters

  • Export feature is limited to visualized meters only.

Zone and usage visualization (2 separate widgets)

  • Widget diagram: up to 8 zones or usages

  • Full screen diagram: up to 20 zones or usages

  • Export feature is limited to visualized zones or usages.

Multi-site comparison view

Schneider Electric recommends up to 50 sites per group to display the multi-site consumption data properly.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.