ESXFEUG003EN-01

Architecture with Com'X Gateway

The following topic presents a typical architecture with a Com'X gateway to cloud using Ethernet network .

This solution offers the following advantages and services:

  • 24/7 notifications to the maintenance team when equipment is no longer supplied.

  • Record of all regulatory maintenance interventions with an associated report.

  • Monitoring of when and where the energy is consumed in the building and over-target consumption alerts.

  • Alerts in case of peaks or low power factor to avoid penalties on the electricity bill.

  • Alerts in case of high harmonics on your electrical network and planning of corrective actions to avoid lighting disturbances.

  • Display of energy savings on a screen at the building entrance (optional).

More Information

For more information about Com'X gateway, refer to the following documents:

Title of documentation Reference number

EcoStruxure™ Power - Commissioning Guide for Connected Panels and Facility Expert Software

ESXP1G004EN

EcoStruxure™ Power - Design & Selection Guide for Energy & Operations Management Solutions

ESXP1G001EN

Com'X 210 Energy Server - User Manual

DOCA0098EN

Com'X 510 Energy Server - User Manual

DOCA0036EN

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.