ESXFEUG003EN-01

Reference Architectures

EcoStruxure Facility Expert cloud-based platform collects energy data from different Schneider Electric gateways depending on the application type and the project size.

  • For large sites and advanced projects, Com'X gateway supports many metering devices types including third party and custom devices.

  • For small businesses, PowerTag Link C gateway connects up to 8 wireless energy sensors with Ethernet connection.

  • For simple and native connectivity, Wireless Panel Server connects up to 15 wireless energy sensors to the cloud through LoRa network.

Each reference architecture presents the system overview, limits, and capabilities.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.