ESXFEUG003EN-01

Using Schedules Data

  1. Select the Schedule entry to analyze the energy consumption of a period according to the calendar and schedules you have set up.
  2. To access more details to review whether the energy consumption is consistent with the building usage, check working/non-working hours consumption for instance, and export data, click More details.
    For more information, see how to create calendar and schedules.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.