ELKO Schneider Charge_WH_00

Firmware auto update

You can choose devices to be automatically updated to the latest firmware. This will give you access to the newest features.
  1. On the Home page, tap All > System Settings > Firmware Updates.
  2. Turn on the toggle for the device for which you want to enable auto firmware update.
This will allow the charger to update to the latest firmware when it becomes available.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.