ELKO Schneider Charge_WH_00

Troubleshooting

Symptom

Possible causes and solutions

Connector plugged into electric vehicle but not charging, LED is solid green.

  • Verify that the connector was inserted properly by unplugging and plugging it back into the socket.

  • Verify the charging sequence by following the procedure described in section "Operation".

Connector plugged into electric vehicle but not charging, LED is blinking blue.

  • Verify that you do not have a schedule in progress through the smart charging application that prevents charging the car.

  • If you have installed the anti-tripping module, it can limit the maximum power drawn by the Schneider Charge, to avoid power outages in your home. Reduce the load consumed by electrical appliances and ensure at least 9 A is available per phase before restarting charging process. Ensure your grid capacity is sufficient for both EV charging and home appliances.

Connector plugged into electric vehicle but not charging, LED is blinking Solid blue.

  • Verify that you do not have a schedule in progress through your car that prevents charging the car.

Charging station's LED breathing Orange.

  • Restart the Schneider Charge.

  • The Schneider Charge is not connected to the domestic network when using Wi-Fi:

    • Verify that you have connected the Schneider Charge to a 2.4 GHz Wi-Fi with WPA2 password.

    • Verify that the Wi-Fi name and password are correct.

    • In case the Wi-Fi signal is too weak: connect the charging station with Ethernet cable, or add a Wi-Fi repeater.

  • Verify that internet router is working properly.

Charging station's LED is blinking red

  • Switch off the power supply to the charging station, unplug the connector from the electric vehicle, reconnect the power supply, wait for the charging station to become ready (LED illuminated solid green), before reconnecting the connector to the electric vehicle.

Charging station's LED off.

  • No power supply. Verify that the cabling is correct and that circuit breaker did not trip.

  • Otherwise, switch off the power supply to the charging station, The charging station is possibly damaged. Please contact Schneider Electric’s Customer Care Centre.

Charging station's LED White light flashing and then power off.

  • Power supply overvoltage seriously (Voltage more than 300V between phase line and neutral line). Switch off the power supply to the charging station, The charging station is possibly damaged. Please check power voltage.

QR code sticker for Wi-Fi access point password is lost.

  • The Wi-Fi access point password to connect eSetup application to perform the configuration or modify the settings can be recovered inside the product by removing the front cover.

PIN code for installer commissioning is lost.

  • A new PIN Code can be created by clicking on "Reset PIN code" and follow the instructions in Wiser Home application.

Main incomer circuit breaker has tripped.

  • Add a anti-tripping module to allow the load shedder.

  • If the anti-tripping module is already installed, check that the setting is correct and that it is correctly paired with the charging station: see anti-tripping module user guide.

  • Add a anti-tripping module (All countries) or connect the TIC to the meter (France only) to allow the load shedder.

  • For TIC version (France Only):

    • Check that the TIC is correctly connected to the charging station by using Wiser Home application.

    • If you have changed your contract from History to Standard, you must restart the charging station to allow the modification in the charging station. It will automatically detect the contract type at each restart.

Connect the charging station to a smart charging application unsuccessfully.

  • When the back-end application requests for the Serial Number, you shall enter the Charger Point Identification number (CPID) that you could find on the side of the charging station.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.