Sensors

SmartSensor Climate Wireless

EKO07219

Maintains a comfortable environment in the home by detecting changes in temperature and humidity and reporting climate data to the hub

Instruction Sheet (PDF)

Device User Guide

SmartSensor Leakage Wireless

EKO07218

Detects the presence of water, and alert via an alarm and/or notification.

Instruction Sheet (PDF)

Device User Guide

SmartSensor Door/Win Wireless

EKO07217

Detects when windows or doors are opened or closed and send the status to the hub.

Instruction Sheet (PDF)

Device User Guide

SmartSensor PIR Wireless

EKO07220

Reports the detection of movement and measures the luminance of the environment.

Instruction Sheet (PDF)

Device User Guide

Motion Sensor Outdoor, 360

EKO025212

EKO025213

It offers advanced motion detection, LUX measurement, and temperature sensing capabilities. It allows you to automate and enhance your smart home environment effortlessly.

Instruction Sheet (PDF)

Device User Guide

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?