990-915656A-001

Clearance

NOTE: Clearance dimensions are published for airflow and service access only. Consult with the local safety codes and standards for additional requirements in your local area.
NOTE: 600 mm (24 in) rear clearance is required for non-routine transformer service such as transformer tap changes.

Minimum Required Clearance for Installation and Operation of the PDU

Minimum Recommended Clearance for Service of the PDU

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?