990-915656A-001

Installation Procedure

Top Cable Entry System

Bottom Cable Entry System

  1. Perform one of the following:
  2. Prepare the PDU for Cables.
  3. Install the Input Cables.
  4. Connect the Load to the Branch Circuit Breakers.
  5. Connect the Ethernet/Modbus Cables.
  6. Final Installation.
For moving or decommissioning the PDU after installation has been completed, see Decommission or Move the PDU to a New Location.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?