990-915656A-001

Connect the Load to the Branch Circuit Breakers

  1. Route the load cables from the load through the top or bottom right side of the PDU. Bottom cable entry is shown in illustration.
  2. For each load cable set:
    1. Connect the N cable to the N busbar.
    2. Connect the ground cable to the grounding busbar.
    3. Route the phase cables (L1, L2, L3) through the provided current transformers for the branch circuit breaker. Check that the direction of the phase cables matches the labels on the current transformers. The signal cables for the current transformers are preinstalled by the factory.
    4. Connect the phase cables (L1, L2, L3) to the branch circuit breaker.

    Front View of the PDU

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?