990-915656A-001

Position the PDU

Installing kick plates and positioning the PDU could also be done during unpacking of the PDU.

  1. Remove the protective packaging bag (A) from the PDU.

    Front View of the PDU

  2. Install the four rear kick plates (2 x TME40741 and 2 x TME40742) on the PDU. Use four screws (provided) to each kick plate.

    Rear View of the PDU

  3. Lift the PDU to the final installation location using a forklift with the required specifications:
    WARNING
    Heavy load
    The product is large and heavy: 4650 kg (10251 lbs). Only lift and move the product using a forklift with the following required specifications:
    • Forklift load capacity: > 5000 kg (11023 lbs)
    • Forklift fork length: > 1400 mm (55.11 in)
    • Forklift fork width (for lifting PDU) : > 1000 mm (39.37 in)
    Failure to follow these instructions can result in death, serious injury, or equipment damage.
    1. Insert the forks in the openings on the front of the PDU. Place the forks as far to the sides as possible as shown.
      NOTICE
      Risk of equipment damage
      The forks of the forklift cannot be inserted completely into the PDU when the rear kick plates are installed.
      Failure to follow these instructions can result in equipment damage.

      Front View of the PDU

    2. Lift the PDU slowly off of the floor. Pay close attention to the balance of the PDU while lifting. Keep a safety distance of 100-130 mm (4-5 in) between the product and the forklift to avoid damaging the product during lifting.
    3. Lower the forks slowly when placing the PDU on the floor.
    WARNING
    Tipping hazard
    • Insert the forks as instructed.
    • Lift and lower the PDU slowly.
    • Pay close attention to the balance of the PDU while lifting.
    Failure to follow these instructions can result in death, serious injury, or equipment damage.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?