990-915656A-001

Environment

  Operating Storage
Temperature -10 °C to 40 °C (14 °F to 104 °F) -25 °C to 55 °C (-13 °F to 131 °F)
Relative humidity 10 to 70% non-condensing 10 to 80% non-condensing
Elevation 0 m to 2011 m (0 feet to 6600 feet) above sea level
0-10000 m (0-32000 ft)
Audible noise one meter (three feet) from unit As per NEMA ST20
Protection class NEMA type 1, external doors with inner dead front panels
Cooling Front, rear, and roof ventilation
Color

APC raven black

Accessibility Front access for:
  • Display

  • Fuse panel

  • Communication and monitoring

  • Adding/replacing branch circuit breakers

Heat Dissipation

Heat dissipation in BTU/hr 44445
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?