990-915656A-001

Compliance

Safety

UL 891, SWITCHBOARDS, Edition 12, Issue Date 07/19/2019

CSA C22.2 No. 244, Switchboards, Edition 2, Issue Date 07/2019

UL 62368-1, Audio/Video, Information and Communication Technology Equipment - Part 1: Safety Requirements, Edition 3, Revision Date 10/22/2021

CSA C22.2 No. 62368-1:19, Audio/Video, Information and Communication Technology Equipment - Part 1: Safety Requirements, Edition 3, Revision Date 10/22/2021

Marking cULus
Performance Transformer DOE2016
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?