Final Installation
![]() |
---|
HAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASH
All panels and covers must be properly reinstalled prior
to energizing the PDU.
Failure to follow these instructions will result in death or serious injury.
|
- Clean/vacuum the PDU of any debris and foreign objects.
- Install the front anchoring brackets on the PDU. The front anchoring brackets were removed during unpacking of the PDU.
- Reinstall the three front plates on the PDU.
- If removed, reinstall the small front plate.
- If removed, reinstall the three side plates on the PDU.
- Install the provided kick plates (TME40751, TME40752, TME40753) on the front of the PDU. Use four screws (provided) for each kick plate.
- Mount the front anchoring brackets to the floor. Use appropriate hardware for the floor type – the hole diameter in the bracket is ø14 mm. Minimum requirement is M12 strength grade 8.8 hardware.
- Remove the two wooden plates from the top of the PDU.
- Install the two roof assemblies:
- Roof assembly 1: Assemble the parts 1x TME69096, 1x TME69194, and 1x TME69105 with the four provided M6x16 screws as shown.
- Roof assembly 2 : Assemble the parts 1x TME69096, 1x TME69236, and 1x TME69105 with the four provided M6x16 screws as shown.
- Place roof assembly 1 (marked (A) in the illustration) and roof assembly 2 (marked (B) in the illustration) on top of the PDU and slide them one by one into the slots in the rear brackets.
- Fasten the roof assemblies to the top of the PDU with the four provided M6x20 bolts with washers.
- Close the front doors and lock with the provided key. Store the key in a safe location where only authorized personnel have access.