990-915656A-001

Install the Input Cables

  1. Route the equipment grounding conductor through the top or bottom left side of the PDU and connect to the grounding busbar.
  2. Route the input cables through the top or bottom left side of the PDU and connect to the input busbars (L1, L2, L3).

    Front View of the PDU

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?