990-915656A-001

Prepare the PDU for Cables

NOTE: Unlock the front doors with the provided key and keep the key in a safe location during the installation.
  1. Open the middle front door and Lockout/Tagout the main input switch MIS/main input circuit breaker MIB in the OFF (open) position. Close the middle front door.

    Front View of the PDU

  2. Open the left and right front doors.
  3. Remove the three front plates. Store the three front plates safely until reinstallation.

    Front View of the PDU

  4. Optional: If you have free space to the right of the PDU, you can remove the three side plates for better access. Store the three side plates safely until reinstallation.
  5. For top cable entry:
    1. Remove the four top gland plates.

      Front View of the PDU

    2. Drill/punch holes for power cables/conduits in the gland plates. Conduits are not provided.
      DANGER
      Hazard of electric shock, explosion, or arc flash
      • Do not drill or punch holes for cables or conduits with the gland plates installed and do not drill or punch holes in close proximity to the PDU.
      • Ensure that the holes do not have sharp edges that can damage the cables.
      Failure to follow these instructions will result in death or serious injury.
    3. Reinstall the four top gland plates.
  6. For bottom cable entry:
    1. Remove the small front plate.

      Front View of the PDU

    2. Remove the four bottom gland plates.

      Front View of the PDU

    3. Drill/punch holes for power cables/conduits in the gland plates. Conduits are not provided.
      DANGER
      Hazard of electric shock, explosion, or arc flash
      • Do not drill or punch holes for cables or conduits with the gland plates installed and do not drill or punch holes in close proximity to the PDU.
      • Ensure that the holes do not have sharp edges that can damage the cables.
      Failure to follow these instructions will result in death or serious injury.
    4. Reinstall the four bottom gland plates.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?