990-6317F-001

Environment

  Operating Storage
Temperature -10 °C to 40 °C (14 °F to 104 °F) -25 °C to 55 °C (-13 °F to 131 °F)
Relative humidity 10 to 95% non-condensing 10 to 90% non-condensing
Elevation 0 m to 2011 m (0 feet to 6600 feet) above sea level
152 m below to 7620 m above sea level
(500 feet below to 25,000 feet above sea level)
Protection class NEMA type 1, solid roof, external doors with inner dead front panels
Cooling Front ventilation (top and bottom)
Color RAL 9003 white for GRPPNF84, GRPPIP2X84, and GRPPNF84
Raven black for GRPPNQ89, GRPPIP2X89, and GRPPNF89
Accessibility Front access for:
  • Display

  • Fuse panel

  • Communication and monitoring

  • Adding/replacing branch breakers

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?