990-6317F-001

Weights and Dimensions

Commercial reference Weight kg (lbs) Height mm (in) Width mm (in) Depth mm (in)
GRPPNQ84 200-250 (441-551) 2134 (84) 610 (24) 305 (12)
GRPPIP2X84
GRPPNF84
GRPPNQ89 2261 (89)
GRPPIP2X89
GRPPNF89
NOTE: Weights depend on selected options. The weights and dimensions above are for one cabinet – the final RPP solution may consist of several cabinets.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?