990-6317F-001

Model List

  • White cabinet, 84 inches tall, 240 V, NQ panelboard, 250 A or 400 A rated (GRPPNQ84)

  • White cabinet 84 inches tall, 240 V, IP2X finger safe panelboard, 250 A or 400 A rated (GRPPIP2X84)

  • White cabinet 84 inches tall, 480 V, NF panelboard, 250 A or 400 A rated (GRPPNF84)

  • Black cabinet, 89 inches tall, 240 V, NQ panelboard, 250 A or 400 A rated (GRPPNQ89)

  • Black cabinet, 89 inches tall, 240 V, IP2X finger safe panelboard, 250 A or 400 A rated (GRPPIP2X89)

  • Black cabinet, 89 inches tall, 480 V, NF panelboard, 250 A or 400 A rated (GRPPNF89)

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?