990-6317F-001

Overview

All options and configurations are selected on ordering and factory-installed to deliver an RPP solution that meets your requirements. The RPP solution consists of a cabinet with main input device(s) and panelboard(s). An extra cabinet can be added to the RPP solution, either empty or with additional main input device(s) and panelboard(s).

See Hardware Options for feature details.

NOTE: A single main input device can feed both panelboards in the RPP. The RPP maximum output current is given by the rating of the main input device.

Overview of Model Options

Commercial reference GRPPNQ84 GRPPIP2X84 GRPPNF84 GRPPNQ89 GRPPIP2X89 GRPPNF89
Input voltage 240 V x x   x x  
480 V     x     x
Main input device 250 A MCCB x x x x x x
400 A MCCB x x x x x x
Panel boards* 1 x NQ42 x     x    
2 x NQ42 x     x    
1 x NQ84 x     x    
1 x NF42     x     x
2 x NF42           x
1 x NF84     x     x
1 x IP2X 42   x     x  
2 x IP2X 42   x     x  
Extra cabinet (empty or for additional main input device(s) and panelboard(s) x x x x x x
Main input device terminals Mechanical lugs x x x x x x
Compression lugs x x x x x x
Cable entry Top x x x x x x
Bottom x x x x x x
Surge protection* 100 kA per phase x x x x x x
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?