990-91381D-001

Install Busbars for Load Bank Breaker (Option)

NOTE: The busbars for the load bank breaker were removed from the UPS during preparation for installation.
  1. Install busbars for load bank breaker (LBB) in the UPS. Note the direction of the busbars.

    Front View of the UPS

  2. The load bank breaker cables can be routed through the top of the UPS for a permanent installation or through the open inner door for a temporary installation. See the UPS manual for information on how to create top cable entry in the UPS.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.