990-91381D-001

Prepare for Signal Cables in Bottom Cable Entry Systems

DANGER
hazard of electric shock, explosion, or arc flash
Do not drill or punch holes with the gland plates installed and do not drill or punch holes in close proximity to the cabinet.
Failure to follow these instructions will result in death or serious injury.
  1. Remove the covers.
  2. Prepare for signal cables:
    1. Remove the gland plates.
    2. Drill/punch holes for signal cables or grommets in the gland plate. Install grommets (not provided), if applicable.
    3. Reinstall the gland plates.
  3. Route the signal cables from the UPS, into the maintenance bypass cabinet, and out through the bottom of the maintenance bypass cabinet.
  4. Reinstall the covers.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.