990-94386-001

Common Lithium-ion Battery

Common Lithium-ion battery configuration (LIBSESMG17UL) is supported.

The battery solution for the 1600 kW UPS system consists of minimum 8 and maximum 10 Galaxy Lithium-ion battery cabinets (LIBSESMG17UL).

The battery solution for the 1800 kW UPS system consists of minimum 9 and maximum 10 Galaxy Lithium-ion battery cabinets (LIBSESMG17UL).

The battery solution for the 2000 kW UPS system consists of 10 Galaxy Lithium-ion battery cabinets (LIBSESMG17UL).

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?