990-94386-001

Common VRLA Battery

Common VRLA battery configuration is supported.

End of Discharge Voltage for VRLA Battery

The voltage is 1.6 to 1.75 per cell depending on discharge ratio.

Standard VRLA Voltage Levels

NOTE: Specific configurations may differ from the general constraint shown above.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?