990-94386-001

Compliance

Safety

UL 1778 5th edition

CSA C22.2 NO. 107.3-14, 3rd Edition

EMC/EMI/RFI Individual UPS cabinets tested for FCC Part 15 Subpart B, Class A
Performance

Individual UPS cabinets: Performance in accordance with: IEC 62040-3: 2021-04, 3rd edition Uninterruptible Power Systems (UPS) - Part 3: Method of specifying the performance and test requirements.

Output performance classification (according to IEC 62040-3, Clause 5.3.4): VFI-SS-11

Transportation Individual UPS cabinet: IEC 60721-4-2 Level 2M2
Seismic ICC-ES AC 156 (2018); OSHPD Pre-approved; Sds=1.28 g for z/h=1 and Sds=1.9 g for z/h=0; Ip=1.5
Earthing system* TN-S, TNC-S
Overvoltage category

This UPS is OVCII compliant.

If the UPS is installed in an environment with an OVC rating higher than II, an SPD (surge protection device) must be installed upstream of the UPS to reduce the overvoltage category to OVCII.

Protective class I
Pollution degree 2
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?