990-94386-001

Derating Due to Load Power Factor

0.5 leading to 0.5 lagging without derating.

UPS rating UPS output
Lagging Leading

PF=1

PF=0.5

PF=0.6

PF=0.7

PF=0.8

PF=0.9

PF=0.9

PF=0.8

PF=0.7

PF=0.6

PF=0.5

1600 kW/ kVA

1600 kVA / 800 kW

1600 kVA / 960 kW

1600 kVA / 1120 kW

1600 kVA / 1280 kW

1600 kVA / 1440 kW

1600 kVA / 1440 kW

1600 kVA / 1280 kW

1600 kVA / 1120 kW

1600 kVA / 960 kW

1600 kVA / 800 kW

1800 kW/ kVA

1800 kVA / 900 kW

1800 kVA / 1080 kW

1800 kVA / 1260 kW

1800 kVA / 1440 kW

1800 kVA / 1620 kW

1800 kVA / 1620 kW

1800 kVA / 1440 kW

1800 kVA / 1260 kW

1800 kVA / 1080 kW

1800 kVA / 900 kW

2000 kW/ kVA

2000 kVA / 1000 kW

2000 kVA / 1200 kW

2000 kVA / 1400 kW

2000 kVA / 1600 kW

2000 kVA / 1800 kW

2000 kVA / 1800 kW

2000 kVA / 1600 kW

2000 kVA / 1400 kW

2000 kVA / 1200 kW

2000 kVA / 1000 kW

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?