990-91379C-001

Configure the Breakers

NOTE: This configuration is mandatory for correct UPS operation.
  1. Tap Configuration > Breakers .
  2. Tap the different breakers in the mimic diagram to configure which breakers are present in the UPS system. Square with a means that the breaker is present, empty square means that the breaker is not present. BF2 presence can only be configured by Schneider Electric Service.
    NOTE: The UPS can monitor up to four battery breakers in a battery solution. The mimic diagram only shows one battery breaker BB even if more battery breakers have been connected and configured for monitoring. If one or more of the monitored battery breakers are in the closed position, the BB on the mimic diagram will show as closed. If all of the monitored battery breakers are in the open position, the BB on the mimic diagram will show as open.
  3. Tap OK to save your settings.
QR code for this page

Was this helpful?