990-91138A-001

Unpack the Maintenance Bypass Cabinet

NOTICE
RISK of equipment damage
Do not unpack the cabinet before the time of installation.
Failure to follow these instructions can result in equipment damage.
NOTICE
RISK of equipment damage
  • Ensure that the floor is level and can support the weight of the jack when it carries the cabinet.
  • Be careful not to damage the cabinets when using the jack.
Failure to follow these instructions can result in equipment damage.
  1. Remove all the packaging, retrieve the installation kits, and save the protective packaging bag for later use.
  2. Remove the front door.
  3. Remove the left, right, and middle pallet parts.

    Rear View

  4. Remove the rear pallet part:
    1. Place the floor protection plate under the pallet on the rear side of the cabinet.
    2. Remove the bolts from the transportation bracket.
    3. Place the jack into the transportation bracket hole and use a drilling machine to lift the cabinet up to the max height of the jack.
      WARNING
      hazard of serious injury
      Do not put your hands or feet under the cabinet while removing the pallet.
      Failure to follow these instructions can result in death, serious injury, or equipment damage.

      Rear View

    4. Remove the rear pallet part.

      Rear View

    5. Use the drilling machine on the jack to lower the cabinet down to the floor.
  5. Remove the front pallet part:
    1. Place the floor protection plate under the pallet on the front side of the cabinet.
    2. Remove the bolts from the transportation bracket.
    3. Install the small bracket for the jack on the front transportation bracket.
    4. Place the jack into the transportation bracket hole and use a drilling machine to lift the cabinet up to the max height of the jack.
      WARNING
      hazard of serious injury
      Do not put your hands or feet under the cabinet while removing the pallet.
      Failure to follow these instructions can result in death, serious injury, or equipment damage.

      Front View

    5. Remove the front pallet part.
    6. Use the drilling machine on the jack to lower the cabinet down to the floor.
  6. Remove the front and rear transportation brackets and the floor protection plate.
  7. Reinstall the front door.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.