990-91138A-001

Interconnect the UPS and the Maintenance Bypass Cabinet

  1. Reinstall the top cover on the maintenance bypass cabinet with four screws.
  2. Remove the three M6 x 16 mm interconnection screws from the left side of the maintenance bypass cabinet. Save for interconnection.
  3. Position the UPS close to the maintenance bypass cabinet with a little free space between the cabinets.
  4. For bottom cable entry only: Remove the preinstalled DC cables from the maintenance bypass cabinet. DC cables are connected directly in the UPS for bottom cable entry.
  5. Route the preinstalled power cables from the maintenance bypass cabinet into the UPS. These preinstalled power cables must be connected in the UPS – follow the UPS installation manual to connect them correctly.

    Front View of the UPS and the Maintenance Bypass Cabinet

  6. Push the UPS into place up against the maintenance bypass cabinet. The rear bracket on the maintenance bypass cabinet must connect to the UPS.

    Rear View of the Maintenance Bypass Cabinet and the UPS

  7. Install the three M6 x 16 mm interconnection screws between the UPS and the maintenance bypass cabinet as shown.

    Front View of the UPS and the Maintenance Bypass Cabinet

  8. Lower the front and rear leveling feet on the UPS and the maintenance bypass cabinet with a wrench until they connect with the floor. Use a bubble-leveler to check that the UPS and maintenance bypass cabinet are level.

    Front View of the UPS

    CAUTION
    Tip hazard
    Do not move the cabinet after the leveling feet have been lowered.
    Failure to follow these instructions can result in injury or equipment damage.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?