990-91138A-001

Installation Procedure

Top Cable Entry System

Bottom Cable Entry System

  1. Follow the unpacking label on the cabinet packaging or see Unpack the Maintenance Bypass Cabinet depending on your model.
  2. Prepare the Maintenance Bypass Cabinet for Cables.
  3. Install the Seismic Anchoring (Option).
  4. Interconnect the UPS and the Maintenance Bypass Cabinet.
  5. Perform one of the following:
  6. Connect the Signal Cables.
  7. Final Installation.
  8. Follow the UPS installation manual to connect the preinstalled power cables from the maintenance bypass cabinet in the UPS and to complete the rest of the UPS installation.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.