990-91138A-001

System Overview

UIB Unit input breaker
MBB Maintenance bypass breaker
IMB Internal maintenance breaker
UOB Unit output breaker

UPS System with Maintenance Bypass Cabinet with Input Transformer

NOTE: The internal maintenance breaker IMB* in the UPS cannot be used in a system with a maintenance bypass cabinet with transformer and must be padlocked in the open position.

UPS System with Maintenance Bypass Cabinet with Output Transformer

NOTE: The internal maintenance breaker IMB* in the UPS cannot be used in a system with a maintenance bypass cabinet with transformer and must be padlocked in the open position.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.